4/17/2012
Honeywell announced that it has added new flow ranges to its Zephyr™ Analog
and Digital Airflow Sensor portfolio to provide high sensitivity at very low flows – making the sensor portfolio ideal for use in a variety of medical equipment and industrial applications.
Honeywell has added four standard flow ranges between ±50 SCCM and ±750 SCCM to its existing flow range of ±200 SCCM. In addition to the flow ranges, a new port/housing style, the short port fastener mount, has also been added to the portfolio. The extended flow ranges give the Honeywell Zephyr™ the ability to detect low-pressure drops that often occur in medical applications and which can impact patient comfort, and can reduce noise and system wear on components, such as motors and pumps. In industrial applications, lower flow range detection can optimize performance in gas leak detection and clogged HVAC air filter detection.
“With the addition of the new airflow ranges, Honeywell provides its customers with more options to integrate the sensor into their application,” said AJ Smith, director of global product marketing for Honeywell Sensing and Control. “Customers will also benefit from the portfolio’s industry-leading accuracy and the ability to customize the sensor to meet their specific application needs.”
Customers who have already designed a bypass that extends the flow range above the normal range of the existing airflow sensor can now use the Honeywell Zephyr™ airflow sensor to optimize overall performance and reduce manufacturing costs.
Additional industry-leading features of the Honeywell Zephyr™ airflow portfolio include:
- Total Error Band as low as ±2.25 %FSS (full scale span) allow for very accurate airflow measurement
- Stability reduces errors due to thermal effects and null shift, providing accurate readings over time and often eliminating system calibration after PC board mount
- Linear output provides a more intuitive signal than the raw output of basic airflow sensors, helping to reduce production costs and design and implementation time
- Low pressure drop typically improves patient comfort in medical applications, and reduces noise and system wear on other components such as motors and pumps
Potential applications for the Honeywell Zephyr™ airflow sensors include:
Medical:
- anesthesia
- hospital diagnostics (spectrometry/gas chromatography)
- nebulizers
- oxygen concentrators
- patient monitoring
- sleep apnea
- spirometers
- ventilators
- ventricular assist devices
Industrial:
- air-to-fuel ratio
- analytical instrumentation (spectrometry, chromatography)
- fuel cells
- gas leak detection
- gas meters
- HVAC filters
- VAV system on HVAC systems
- meteorology
Please see the following for additional information from Honeywell Sensing and Control: